STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FD CAN doesn't work properly

What is the best way to set up FD CAN in classic mode on stm32 nucleo h743zi board?Currently, I'm using FDCAN with 16 Mhz frequency on the bus and I want to get 500kbit/s.My settings are:hfdcan1.Init.NominalPrescaler=2;hfdcan1.Init.NominalSyncJumpWid...

MKami.0 by Associate
  • 1297 Views
  • 1 replies
  • 0 kudos

STM32F4: Waking from sleep, can't get HSE/PLL running

I'm toggling an I/O in the SYSTICK interrupt every 0.5 seconds with the processor running at 168MHz and using an RTC interrupt to wake the CPU from sleep. This all works well and the processor wakes up after the programmed interval. As per the HAL ...

Mask interrupt temporary

Hi All,I need to enable interrupt on GPIO PC0 only for 1sec: before and later interrupt form PC0 must be ignored.I've tried with disable the interrupt at the init and enable in a thread, wait for 1 sec and then disable again, but it doesn't work!stat...

Multichannel ADC using DMA not working on STM32F429ZI-Disco1

static void MX_ADC1_Init(void) {   /* USER CODE BEGIN ADC1_Init 0 */   /* USER CODE END ADC1_Init 0 */   ADC_ChannelConfTypeDef sConfig;   /* USER CODE BEGIN ADC1_Init 1 */   /* USER CODE END ADC1_Init 1 */ /** Configure the global featur...

MFaro by Associate
  • 882 Views
  • 0 replies
  • 0 kudos

Any indicator for why STM32 leaves SLEEP / STOP Mode?

I'm using the STM32L152. At certain points in my code I go into STOP mode. It seems to come out immediately. I'm not sure what interrupt or event is causing this. Is there any indication somewhere what event caused the processor to change modes? Than...

LThal by Associate III
  • 1449 Views
  • 3 replies
  • 0 kudos

STM32F303 ADC Simultaneous 4 ADC sampling

Hello ,I have recently bought a Nucleo-144 with an STM32F303ZE . Ive been testing out basic programmes including ADCs and I am new to STM32 and embedded in general .Problem:I need to sample 4 channel input Intermediate Frequency(2MHz signal , and i ...

USakt by Associate
  • 1285 Views
  • 0 replies
  • 0 kudos

How to wake up from stop mode with alarm A?

Hello, I'm trying to wake up from stop 1 with the alarm A, and I was wondering if someone can help me with this. Here is my code (I'm using HAL libraries first, the "easy" way base on the example ST gives: PWR/STOP1_RTC):...int main(void){ GPIO_Ini...

Emm1592 by Associate II
  • 1770 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.