2019-04-23 12:03 AM
What is the best way to set up FD CAN in classic mode on stm32 nucleo h743zi board?
Currently, I'm using FDCAN with 16 Mhz frequency on the bus and I want to get 500kbit/s.
My settings are:
hfdcan1.Init.NominalPrescaler=2;
hfdcan1.Init.NominalSyncJumpWidth=1;
hfdcan1.Init.NominalTimeSeg1=13;
hfdcan1.Init.NominalTimeSeg2=2;
hfdcan1.Init.DataPrescaler=1
hfdcan1.Init.DataSyncJumpWidth=2;
hfdcan1.Init.DataTimeSeg1=13;
hfdcan1.Init.DataTimeSeg2=2;
Using osciloscope I see that one bit is sending in 13 ms time, when it should be in 2 us.
How to set things up properly?
2019-04-23 3:38 AM
Hello,
I recommend you to follow the FDCAN example within STM32CubeH7, shows how to configure the FDCAN peripheral to send and receive
Classic CAN frames in normal mode:
STM32Cube_FW_H7_V1.3.2\Projects\STM32H743I_EVAL\Examples\FDCAN\FDCAN_Classic_Frame_Networking
Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.