2019-04-22 8:14 AM
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_ChannelConfTypeDef sConfig;
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = ENABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 3;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.EOCSelection = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = 2;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_2;
sConfig.Rank = 3;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */
/* USER CODE END ADC1_Init 2 */
}
int main(void)
{
HAL_Init();
MX_GPIO_Init();
MX_DMA_Init();
MX_DMA2D_Init();
MX_FMC_Init();
MX_GFXSIMULATOR_Init();
MX_I2C3_Init();
MX_SPI5_Init();
MX_TIM1_Init();
MX_USART1_UART_Init();
MX_ADC1_Init();
MX_CRC_Init();
// osKernelStart();
HAL_ADC_Start_DMA(&hadc1, (uint32_t *) ADC_Data,3);
while (1)
{
sprintf(tx_data, "%d", ADC_Data[0]);
sprintf(tx_data_2, "%d", ADC_Data[1]);
sprintf(tx_data_3, "%d", ADC_Data[2]);
HAL_UART_Transmit(&huart1,(uint8_t*)(&tx_data), 13,10);
HAL_UART_Transmit(&huart1,(uint8_t*)(&tx_data_2), 13,10);
HAL_UART_Transmit(&huart1,(uint8_t*)(&tx_data_3), 13,10);
HAL_Delay(500);
}
}
Hi Guys,
I am trying to use Multi-Channel ADC using DMA using STM32F429ZI-DISCO1. What I am doing in above code is to get data from Channel 0,1,2 and send that to UART where I can see the ADC value. But I am only getting data from Channel 0. None of other channels are working. I have tried many approaches suggested on youtube lectures but couldn't solve the problem.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.