STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cheap Evaluation Board with SD-Card

Is there a cheap eval board e.g. Nucleo-64 with an SD-card reader. Also A cheap shield for Nucelo-64 with SD-card socket would be ok.Its for a simple logger application but I am hesitant to make a board for only a uC Sensor and SD-Card.

stephan2 by Associate II
  • 1646 Views
  • 2 replies
  • 0 kudos

How to use SPI + DMA in Full Duplex Mode

Hey guys,I'm currently struggling to setup my SPI to work in Full Duplex Mode together with an DMA.I'm using 2 STM32F4 to communicate via SPI + DMAThe Initialization for both MCUs was created using STM32Cube.This is the generated Init Code for the ma...

JHeni by Associate II
  • 6321 Views
  • 3 replies
  • 0 kudos

want to use 'stm32f407' to communicate with Lin.

Hello.I want to use 'stm32f407' to communicate with Lin.There are many difficulties because there are no example sources.Only errors occur when data is sent.If anyone has succeeded in lin, please help me.Give me a simple example of sending and receiv...

HG LEE by Associate II
  • 800 Views
  • 0 replies
  • 0 kudos

Support for accessing SD card through SDIO/SPI interface through Keil platform or a firmware coding model?

The device we are using is STM32F446RE nucleo board.We would like to have well documented support for accessing SD card through either of these two modes:i.SDIO mode(1-bit)ii.SPI modeWe have tried tweaking the code provided for other variants in STM ...

How to use 2 gpio interrupts on same EXTI2 line

Hi ,I have connected switch to PC2 and PD2 (the are acting as gpio input),after trying to generate initial code using cubemx found that these two pins are on same gpio interrupt EXTI2 line , so cubemx is not allowing to have interrupt on both pins,is...

SA.17 by Associate III
  • 3158 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.