2019-05-16 6:53 AM
Is there a cheap eval board e.g. Nucleo-64 with an SD-card reader. Also A cheap shield for Nucelo-64 with SD-card socket would be ok.
Its for a simple logger application but I am hesitant to make a board for only a uC Sensor and SD-Card.
2019-05-16 6:58 AM
The less expensive is the 32F469IDISCOVERY
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-05-16 7:19 AM
> Also A cheap shield for Nucelo-64 with SD-card socket would be ok.
Nucleo-64 has Arduino UNO compatible connectors, I'm sure you can find a SD Card (or microSD Card) shield for Arduino and just use it on Nucleo-64. Sparkfun has them, but they are not exactly cheap, so maybe you'll find a cheap one in one of the Chinese stores. In any case, make sure to double-check if the pinout is compatible with Nucleo.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.