STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error initializing uart2 for STM32F072CBT6 processor

We wanted to use the uart2 serial port of STM32F072CBT6. We used the STM32CUBE tool to generate the code, but the debugging found that we could not enter the interrupt of uart2.We had no problem setting uart1 and uart3 to use before.The initializati...

mhou by Associate II
  • 4026 Views
  • 9 replies
  • 0 kudos

CACHEING OF BACKUP RAM

With the data cache enabled is the backup ram cached such that an Invalidate Cache instruction is required to write the data through?

STM32L433xx/STM32L443xx Errata sheet (ES0318) rev 4 typo

This is a minor thing, but.... STM32L433xx/STM32L443xx Errata sheet, ES0318, revision 4, section 2.1.2 on VDIV/VSQRT says there are two work possible arounds, but then lists the same work around 2 times (disable lazy FPU context save). What is the ...

Bob S by Super User
  • 817 Views
  • 0 replies
  • 0 kudos

Help with ADC and DMA

I'm using a Nucleo-H743ZI and have configured ADC3 to trigger off of TIM3. It is scanning 4 channels every 10 us. I also have BDMA configured for the ADC. The ADC end-of-scan interrupt is occurring every 10 us, but the DMA interrupt is only occurr...

edwin8 by Associate II
  • 3845 Views
  • 7 replies
  • 0 kudos

Measure time difference between 2 PWM using STM32L4

Hi Guys,I working on a project that require measure time difference between 2 PWM (Refer the picture below) . I was able to measure the PWM frequency using input capture method but not able to measure the time difference, Td between 2 PWM. Kindly nee...

LXian.19 by Associate
  • 1284 Views
  • 2 replies
  • 0 kudos

FOC SDK Private Libraries

I see that some libraries from the SDK (Like the PLL State Observer) are delivered as precompiled objects for each of the supported IDE's. Is it possible to obtain the source code of these libraries in order to use them in our project's IDE? (Since w...

kswarm by Associate II
  • 2965 Views
  • 6 replies
  • 1 kudos

Resolved! Why cant debug the nucleo board

Hi, I am learning how to use Uart and created a simple example project where I sent 'hello world'. i then use RealTerm to view this message. i have generated this project using CubeMX and it works however i flashed the board once and after that i can...

MikeP by Senior
  • 1706 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.