STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F769i board novice question

Hi Community,I try to develop my first test app for the STM32F69i board. I got STM32CubeIDE environment working, generated project with all the default settings for this board. According to STM32F769i docs user LED1 and 2 are hooked up to port J, pin...

TDJ by Lead
  • 722 Views
  • 2 replies
  • 0 kudos

ADC3 on STM303F3xx not working (PB0, PB1).

I have an old project already using PA 0,1,2,3,5,7 and PC 1,2,3 as analogue inputs, all on ADC 1 and 2. Due the nature of the project I read some of them in a interrupt timer, and some on demand,when a UART command kicks in. I had to add 3 more ADC's...

Marius CO by Associate III
  • 765 Views
  • 0 replies
  • 0 kudos

Resolved! Help configuring STM32H7 timer

On the Nucleo-H743ZI board, I'm trying to configure TIM3 with a 10 us period. With the internal clock source at 200MHz, I would expect these parameters to create a 10 us TIM3 interrupt:htim3.Instance = TIM3; htim3.Init.Prescaler = 200; htim3.Init...

edwin8 by Associate II
  • 3713 Views
  • 4 replies
  • 0 kudos

How to use QSPI as Single SPI mode?

I am using STM32F779BI for my custom board. I am using TFT LCD Display connected to QSPI, but I want to use QSPI in single SPI Mode. Like simple SPI ( CLK, MOSI, MISO).How to initialize QSPI in Single SPI Mode?

Resolved! STM32F446 FMC SDRAM and linker script

Dear,For the first time, i use an external SDRAM with the FMC peripheral of the STM32F446.I succeeded to describe a in the linker script to place specific data in this section.BUT this section is present in the output file (.hex) when I build my code...

YDann.7 by Associate III
  • 3088 Views
  • 5 replies
  • 0 kudos

STM32F7, 32-bit timer from 2x 16 bit timers on APB2

Hi,I need a faster 32-bit timer (TIM2 and TIM5 which are 32-bits are on 108MHz AHB1). So idea is to chain 2x 16 bit timers on APB2, choose TIM1 and TIM8. But I just can't configure it to work as it should using CubeMX. I'm also not sure how to adjust...

MBo�?.7 by Associate II
  • 5841 Views
  • 11 replies
  • 0 kudos

STM32L052C8 I2C Communication issue

We are interface AT24C512 EEPROM with STM32L052C8 but there are problem facing in i2c communication. we are using STMCubeMx for generate i2c library.here, STM32L052C8 as Master and AT24C512 EEPROM as a Slave.we are calling I2c Function HAL_I2C_Mem_Wr...

DTimb by Associate
  • 902 Views
  • 0 replies
  • 0 kudos

Interrupt RX isn't called on STM32F413ZH Nucleo board

What is wrong with the following code that the RX Interrupt isn't called. On the osziloscope I see Send and Receive correctly.HAL_Init();__HAL_RCC_GPIOA_CLK_ENABLE();__HAL_RCC_USART6_CLK_ENABLE();#define CONSOLE_TXD_PIN LL_GPIO_PIN_11/* Configure T...

MKubi by Associate
  • 856 Views
  • 0 replies
  • 0 kudos

I have STEVAL-IDP005V1 and Nucleo64 boards and STEVAL-IDP005V1 already programmed, i interface the specified devices together but not able to get the output on serial monitor

The STEVAL-IDP005V1 is already programmed with Condition Monitoring firmware and i connect the STEVAL-IDP005V1 to st-link on stm32 nucleo board, when i copy the .bin file it raises an error & some times not, but am not able to see the output. please ...

v_1 by Associate II
  • 622 Views
  • 0 replies
  • 0 kudos

HOW TO DOWNLOAD FIRMWARE .BIN FILES FOR STM32 MCUs ?

https://www.st.com/content/ccc/resource/sales_and_marketing/presentation/product_presentation/group0/47/a2/91/a0/fe/ca/42/89/steval-bfa001v1b_getting_started_guide/files/steval-bfa001v1b_quick_start_guide.pdf/jcr:content/translations/en.steval-bfa001...

v_1 by Associate II
  • 1602 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.