STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello All, I am new to this community as well as STM32F407 Discovery board . I am trying to write a program to turn ON LED without using any library. I wrote the below code, But I am not able to compile it .

  #define RCC_AHB1ENR (*(volatile unsigned long *)0x40023830)#define GPIOD_MODER (*(volatile unsigned long *)0x40020C00)#define GPIOD_OTYPER (*(volatile unsigned long *)0x40020C04)#define GPIOD_OSPEEDR (*(volatile unsigned long *)0x40020C08)#define G...

JSuda by Associate II
  • 5096 Views
  • 11 replies
  • 0 kudos

Mass Erase before every FSTPG? (STM32L4SVIT)

Using:STM32L4SVITDBANK=1The reference manual seems to state that a Mass Erase must be performed before every FSTPG. However the requirement is not clear. Assuming it is correct that a Mass Erase is required to use FSTPG: 1.Is there a time window ...

JFieb by Associate II
  • 1087 Views
  • 0 replies
  • 1 kudos

How to detect last used address in flash?

Hi,I would like to detect last used address in flash to be able to backup the firmware from internal flash memory to external from my bootloader. I know the start address where from start copying data, but don't know the end. I was unable to found a ...

Resolved! Why SDIO needs about 3ms on transferring only 512Bytes

Hello, ST experts​STM32F415RGT6 is used on custom board. Everything looks fine except that SDIO opertions. f_write function is called at an interval about 500ms to write 512Bytes to SD card. SDIO_CLK is 24MHz, 4bit bus wide. I really don't know why t...

Yang Yang by Associate III
  • 1137 Views
  • 1 replies
  • 0 kudos

Resolved! PWM RESOLUTION OF STM32F030F4P6TR

Hello, I am new to the embedded community and was facing a problem figuring out the pwm resolution of the STM32F030F4P6TR microcontroller. I went throught the datasheet and the user manual but did not find any solution to my problem.Thanks,Apurv.

AMara by Associate II
  • 1697 Views
  • 4 replies
  • 0 kudos

STM32F7 maximum speed

Recently, I began to deal with the STM32F7 stone, as the STM32F4 lacked speed. By the result, I realized that if you simply run the same program (calculating digital filters) on F4 and F7 at the maximum core frequency, then the performance does not i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.