2019-06-06 1:45 AM
Hello, ST experts
STM32F415RGT6 is used on custom board. Everything looks fine except that SDIO opertions.
f_write function is called at an interval about 500ms to write 512Bytes to SD card. SDIO_CLK is 24MHz, 4bit bus wide. I really don't know why there are activities lasting 3ms on sdio_cmd pin.
Best Regards
Yang
Solved! Go to Solution.
2019-06-06 4:43 AM
Haven't timed it, but single sector writing is very inefficient, there is a lot of command overhead, blocks on the media are typically around 128KB. If your writes aren't aligned FatFs will need to read and write several sectors.
2019-06-06 4:43 AM
Haven't timed it, but single sector writing is very inefficient, there is a lot of command overhead, blocks on the media are typically around 128KB. If your writes aren't aligned FatFs will need to read and write several sectors.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.