STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Rotary Encoder Pulse Count

Is it proper way to to count encoder pulses using rising/falling edge interrupt instead of using Timer in Encoder Mode??Because in my application I need interrupt above 80000 pulse count. But here timer is of 16-bit (STM32F103C8T6) so it can only cou...

JPanc.1 by Associate II
  • 1330 Views
  • 1 replies
  • 0 kudos

STM32F030C8 warm start failure

We have several STM32f030C8s that refuse to start if the ambient temperature is 40deg C. Below, say 20 deg C, they start and continue to run up to and beyond 40 deg c ok. Applying a reset on a stalled processor brings it to life. Is this a known p...

DPidd by Associate II
  • 2381 Views
  • 5 replies
  • 0 kudos

Resolved! Rotary Encoder Application

I am using STM32F103C8T6 for counting rotary encoder pulse.My Encoder PPR is 5000.But when I program for timer1 as encoder mode and show count on segment it shows 20000 pulse per rotation it is 4 times higher than the actual value. What should I do t...

JPanc.1 by Associate II
  • 2179 Views
  • 3 replies
  • 0 kudos

How to do STEP/DIR interface?

Hello,I need to connect STEP/DIR driver (DRV8825 to STM32F103) for driving one axis stepper motor. I will use buttons for moving and I need to set acceleration and deceleration profile. Do you have some experience what way of pulse generation I shoud...

TIM_OCMODE_ACTIVE output problem ?

I config timer'mode is TIM_OCMODE_ACTIVE  , start enable ,can output waveform,but enable more than one time , only output the first corresponding waveform .why behavier so ?but when I config timer TIM_OCMODE_PWM2( or TIM_OCMODE_PWM1 ),enable and di...

Resolved! TIMx Clock Division Configuration

Hey, I am trying to understand timers, everything goes nice, but I have a question in my mind.I am able to set the prescaler and period values according to my purporse, but I can't use the internal clock division effectively.My TIM2 clock signal is 1...

YAkse by Associate III
  • 7460 Views
  • 8 replies
  • 4 kudos

About Timers triger ADC

How to config Timers when I want to use it to triger ADCs, May I get an example?STM32F103​have already been solved

CWang.4 by Associate
  • 693 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.