STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI not working with MCP6S21

Hi everyone,I would like to use a simple VGA (MCP6S21) but still not reach to do it.The datasheet is available here : http://ww1.microchip.com/downloads/en/devicedoc/21117b.pdfI'd like to put a +2 gain, the signals (SCK,MOSI) I transmit seems to be O...

MJouv by Associate
  • 993 Views
  • 0 replies
  • 0 kudos

About UART communication between PC and STM32F4

Hey, I am trying to connect my STM32F4-DISC board to PC via USART. It is a very common and basic example like sending a string to PC COM port which is covered by lots of tutorials on the web. But my question is,I first used this product and directly ...

YAkse by Associate III
  • 1130 Views
  • 1 replies
  • 0 kudos

stm32 write serial number

how to write SN for hundreds MCUS​? i know j-flash can write fixed bytes,i need to write custom 10 bytes SN which has its own generation rule

Using an STM32F031, can I have one ADC channel being monitored by analog watchdog and another channel being scanned in each iteration of the main loop?

Lets say I have channels 1 and 2.I was wondering if I disable continuous scan and enable watchdog on 2. Will the interrupt for channel 2 be called only when I do a start scan or will the watchdog keep continuously checking the channel 2?In other word...

SSudh.12 by Associate
  • 613 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.