STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Cannot Update TIM1 CCR2 for Phase Shift PWM

Dear STM community,I use STM32 nucleo-f303ze with stm32cubeide , I try to achieve 4 PWM complementary signal  with controlled phase shift by potentiometer by using TIM1 channel 1 PWM Generation CH1 CH1N and TIM8 channel1 channel 1 PWM Generation CH1 ...

123.png 122.png

STOP2 Mode in stm32u5g7

Hi I am utilizing an STM32U5G7 microcontroller to operate a BLDC motor with a system clock frequency of 80 MHz. I require assistance in configuring the device to enter and exit Stop2 mode to achieve the lowest power using the RTC wakeup functionality...

_Danny_ by Associate III
  • 1647 Views
  • 3 replies
  • 0 kudos

Clock Gating (I2C HSI kernel clock) prevents Standby

Hi,I have a situation which I would like to understand better:I have an STM32U595ZJT6Q with I2C2 configured to use HSI16 (not PCLK1) as its kernel clock. I put the STM32 into Standby to save power.Recently I implemented Clock Gating to save power whe...

BCowp.1 by Associate II
  • 1243 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 boot mode

Hi,I'm currently working with the STM32G491RET and using the NUCLEO-G491RE evaluation board. I need to check whether the device enters boot mode using the BOOT0 pin and NRST. From my understanding, to enter boot mode, BOOT0 should be driven low, and ...

Occasional jumps during TSC reading

I am working on touch detection with STM32L412cbt6 MCU. I am reading from two channels via G1 of TSC and it is working fine. However, when I look at the other group (i.e. G2), there are fluctuations in both channels from time to time but these values...

xx58 by Associate
  • 1557 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H745i-disco uboot support or device tree

Hi,I'm curently working on a STM32H745i-disco and need to implement a uboot on it. It doesn't seem to be natively supported. I would like to know if there is a port on going or at least if you have somewhere the linux/uboot device tree for this board...

STM32H562 Digital vs Analog temperature sensor

HiWe are currently working on a new board with a STM32H562. As part of the design, we want to measure the temperature of the MCU. In the Datasheet of the STM32H562 I see the “Analog temperature sensor” (as I know it from other STM32) connected to the...

MMeie.3 by Associate III
  • 2629 Views
  • 5 replies
  • 5 kudos

Resolved! First call of timer expires immediately

Hi,I am trying to check if a button is pressed for 3s continuously using a timer which is started through an interrupt. The code for the same is attached below. The issue I am facing is the interrupt is immediately called when I press the button afte...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.