2025-04-24 11:24 AM
Hi,
I'm curently working on a STM32H745i-disco and need to implement a uboot on it. It doesn't seem to be natively supported. I would like to know if there is a port on going or at least if you have somewhere the linux/uboot device tree for this board. Found it for Zephyr but not Linux / uboot.
Thanks in advance.
Solved! Go to Solution.
2025-04-30 5:58 AM
After further investigation. Nothing has been done for this board.
It is nonetheless similar to the stm32h743 I'll give a try to port it, an see what's happening.
2025-04-24 12:06 PM
>>I would like to know if there is a port on going ..
Probably not, this isn't really a suitable Linux target, perhaps look at what ucLinux is doing, or pick a board from the MPU series, ie STM32MP
2025-04-24 12:16 PM
Hi thanks for the fast reply.
I said Linux because the format of the device tree is the same than u-boot. But I mostly focus on u-boot.
And I supposed that maybe ST would have a stm32h745.dtsi , a stm32h745i-disco.dts and in my biggest dreams a stm32h745i-disco-u-boot.dtsi maybe available somewhere. It has been done for the stm32h743i-disco yet.
Thanks
2025-04-30 5:58 AM
After further investigation. Nothing has been done for this board.
It is nonetheless similar to the stm32h743 I'll give a try to port it, an see what's happening.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.