STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Need help to program an STM32F051K8.

I have an STM32F051K8 that I burned out on a Lumenier tx5gs vtx. It still transmits video but I cannot change channels. I thought it would be fun to try and replace it. Fortunately the 3.3v, GND, SWDIO, and SDCLK pins are all broken out on the board....

GWilk by Associate II
  • 1966 Views
  • 4 replies
  • 0 kudos

STMicro announces #PlaysForSure program

Now if we can just get them to perform some rudimentary QA on the software they release we'll be golden.https://www.youtube.com/watch?v=nu2VJBz0MBA&feature=youtu.bePlease get you own house in order before doing this kind of marketing.#PlaysForSure (y...

STM32F429 IAP not working

Hai, I am using stm32f429igt controller I am trying to use IAP and found one example with stm32f4 cube package. While trying the example the code is not getting uploaded when I tried to upload it still waiting for the file can anyone help me how to s...

AChan.15 by Associate II
  • 2439 Views
  • 3 replies
  • 0 kudos

Open-Drain output connected to WKUP pin

Hi,I'm working with an STM32L073RZ on a custom board, using MbedOS 5.12.0 bare metal. The board is a very low power weigh scale that is normally in Standby mode and is awoken by an accelerometer (connected to PC_13), an NFC chip (connected to PA_0). ...

Resolved! STM32F429ZI aborting DMA transfer on USART3 prematurely

On an STM32F429ZI, I'm using USART3_RX to receive information via DMA into a circular buffer. The buffer is 4096 bytes long.If I send 1 or 2 bytes at a time (i.e. with a delay of ~100ms+ between transfers), things work correctly. By "work correctly" ...

TDK by Super User
  • 2313 Views
  • 4 replies
  • 0 kudos

Timer synchronization still has offset

Hello,I am trying to synchronize two PWM outputs on an STM32H7: TIM4 channel 2 and TIM8 channel 3N.To do this I am using the HAL synchronization functions, setting TIM4 up as master with "HAL_TIMEx_MasterConfigSynchronization" and TIM8 with "HAL_TIM_...

ST User by Associate III
  • 2317 Views
  • 3 replies
  • 0 kudos

Where is the VREFINT_CAL for STM32L072z

Hi everyone ! I read in the datasheet that I need the VREFINT_CAL to calculate my real VDDA but I don't find it in the datasheet. In every other model's datasheet you can find the VREFINT_CAL easily but not in the STM32L0 one. Is someone kno...

YMAIL by Associate II
  • 1612 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.