2019-07-11 10:31 AM
Hello,
I am trying to synchronize two PWM outputs on an STM32H7: TIM4 channel 2 and TIM8 channel 3N.
To do this I am using the HAL synchronization functions, setting TIM4 up as master with "HAL_TIMEx_MasterConfigSynchronization" and TIM8 with "HAL_TIM_SlaveConfigSynchronization" in TRIGGER mode.
The timer synchronization works: I can see the rising edges of the PWMs are aligned on an o-scope, however there is still a 2.4 us offset between the rising edges of the two timers. Surprisingly the rising edge of the slave timer occurs first.
What is causing this offset, and is there a way to eliminate it?
My first thought is to set both timers up as slaves and have a separate timer as master to trigger them both to start. I am also wondering if this might be some artifact from synchronizing the outputs of a + channel with a - channel.
Any tips would be appreciated, thank you.
2019-07-11 2:30 PM
> Surprisingly the rising edge of the slave timer occurs first.
Do you enable the slave timer's counter (by setting TIMx_CR1.CEN)?
JW
2019-07-11 2:38 PM
I'm using the HAL functions, in this case HAL_TIMEx_PWMN_Start. Looking at the hal function it does not enable the counter if the slave mode is set to trigger. I may try stepping through in the debugger to verify that it is taking that path.
Do you believe that is the correct procedure: don't enable the counter in trigger mode?
2019-07-12 7:30 AM
I don't use Cube/HAL and don't intend to investigate what its functions do.
The slave timer ought to be enabled by the trigger coming from the master - that's the whole point of the trigger slave mode.
While single-stepping, check if the timers' registers have the expected content. Note, that timers can be stopped or not during the single-step stop, in the respective DBGMCU_APBxFZx register.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.