STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32f411 spi4 low clock speed

Hello!I have problem with spi4 clock speed. I want to drive a lcd tft display but spi clock is max 500Khz, baudrate prescaler set to SPI_BAUDRATEPRESCALER_2. Is very weird. Initial setup was made with CubeMX to 48Mbit/s. APB2 clock is set to 96Mhz. I...

mcufan by Associate III
  • 11066 Views
  • 18 replies
  • 0 kudos

FMC Issue with Allignment

I am trying to read/ write data into FMC SDRAM (16 bit) in Bank 1. While writing the data hard fault occurred. What is the reason for that hard fault, is there any problem with data alignment, If yes what is the solution for it ?

PBU by Associate III
  • 972 Views
  • 1 replies
  • 0 kudos

Interruption each 10 seconds with RTC

Hi guys,I'm using STM32LO and i try to implement a code who aquire data of a sensor every 10 second in a fix day in a week. The rest of the time, the ship is sleeping.I'm trying to do that interruption with RTC and i configure the RTC and program my ...

0690X000009YvlDQAS.png 0690X000009YvlIQAS.png 0690X000009YvlNQAS.png
mibou23 by Associate II
  • 2715 Views
  • 2 replies
  • 0 kudos

STM32L451VC: Problems with ADC.

Hello, I'm working with a PCB based on STM32L451VC MCU and I have different problems with the ADC. I'm trying to measure an input channel using the HALs provided by the STM32CubeMX but I can't achieve it. The main problem is that the bit ADRDY from A...

Luis Ber by Associate II
  • 787 Views
  • 0 replies
  • 0 kudos

Have a question concerning specifically the STM32F479 NRST pin, but this may be applicable to other STM MCU’s as well. Is this Pin an Input/Output pin ?

 I read in section 6.2.1 of the STM32F479 reference manual that this Pin will Output a 20us reset pulse during Watchdog and other internal events. I did not find any Output characteristics for NRST and the statement in section 6.2.1 was stated almost...

JMcHA by Associate
  • 1374 Views
  • 2 replies
  • 0 kudos

Passing parameters from gcc command line

Hi,I'm attempting to pass a parameter for a conditional compile from the gcc command line to my application. I have two build makefiles, one for debug and one for release. We have some code that's only meant for the release build. So far, so good. If...

LThal by Associate III
  • 4772 Views
  • 3 replies
  • 0 kudos

Sine wave interpolation for pwm generation

Hey everyone,I'm still busy scoping out how to do this. I've been looking int methods to generate sine waves and so far it looks like some of the methods use lookup tables or trig functions from cmsis.Although I don't think this would be very ideal, ...

con3 by Senior
  • 5408 Views
  • 5 replies
  • 0 kudos

115200 and 230400 baudrate ?

Dear Members,Is it fast enough to sample 115200 bps with 230400 ?Is it possible to get 230400 bps with 2.097MHz APB ? or I need more ?thanks

STM32H743 FDCAN Communication problem in classic mode

Hey guys,I have this project with STM32H743 MCUs one board uses ZI and second VI version. Sources for both boards were generated in CubeMX.After many unsuccessful attempts to get these two boards talking to each other via classic CAN I replaced one o...

PMego by Associate
  • 1843 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.