2019-07-19 2:11 PM
Hello!
I have problem with spi4 clock speed. I want to drive a lcd tft display but spi clock is max 500Khz, baudrate prescaler set to SPI_BAUDRATEPRESCALER_2. Is very weird. Initial setup was made with CubeMX to 48Mbit/s. APB2 clock is set to 96Mhz. I tried with dma, and without hal but the speed remains the same
What is the cause of this very low spi clock output speed?
Solved! Go to Solution.
2019-07-20 5:24 AM
As you can see, although PLL is switched on in CR, PLLCFGR is at its default value; nonetheless your system clock is set to HSI in CFGR, and both APB dividers are set to 16 (maximum).
In other words, you don't run the SystemClock_Config() function as you've presented us above. Find out, how do you actually set the clocks.
JW
2019-07-19 2:24 PM
Your clocks are wrong?
printf("%d\n", SystemCoreClock);
Output internal clock via MCO/PA8 and scope that against SPI Clock, and attach.
2019-07-19 3:00 PM
Is not wrong. HSE_VALUE = 8000000
i check with assert in early main. The SystemCoreClock is 16000000 but not think is a problem, if i set to 8000000 the spi working the same
2019-07-19 4:02 PM
printf("HCLK=%d\n", HAL_RCC_GetHCLKFreq());
printf("APB1=%d\n", HAL_RCC_GetPCLK1Freq());
printf("APB2=%d\n", HAL_RCC_GetPCLK2Freq());
Make sure to clear the initialization structures for the SPI4
2019-07-20 1:25 AM
with printf:
HCLK=16000000
APB1=1000000
APB2=1000000
what do you mean clear the initialization structures for the SPI4?
2019-07-20 1:34 AM
here my clock config:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/**Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 192;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 8;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
PeriphClkInitStruct.PLLI2S.PLLI2SN = 200;
PeriphClkInitStruct.PLLI2S.PLLI2SM = 5;
PeriphClkInitStruct.PLLI2S.PLLI2SR = 2;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
2019-07-20 2:06 AM
> spi clock is max 500Khz,
And you know that how?
JW
2019-07-20 2:28 AM
no idea..
the HAL_RCC_GetPCLK2Freq() give me 1000000Hz
very strange..
2019-07-20 2:33 AM
So SPI4 clock half of APB clock. Not sure why we are at 1 MHz for those.
= {0}; // clears auto variables on stack
2019-07-20 2:53 AM
And what's the actual SPI clock, as measured on the SCK pin?
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.