STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 Flash programming issue

​Hi,on a stm32h743 (with IAR embedded workbench IDE Version 8.30.1) i am experiencing the following Problem in the HAL_FLASH_Program function:The Input Parameter DataAddress is reinterpreted as uint64_t* and copied to the Destination by the line*dest...

EStei.3 by Associate III
  • 2408 Views
  • 1 replies
  • 0 kudos

STM32F722VET6 MCU Malfunctioning

We are using STM32F722VET6 MCU in one of our project.Memory defined are in linker as below:RAM : 256KBROM : 512KBStack : 4KBWe have configured below peripherals and developed an application code using user defined functions. Which is working as exp...

SPate.14 by Associate
  • 2394 Views
  • 2 replies
  • 0 kudos

Resolved! Recognizing SPI data reception in STM32F429

I'd like to ask how the STM32F429 recognizes data reception in case of SPI while there is no any start bit? I know that there is RXNE bit in SPI_SR status register, but how SPI knows where is the first bit of the transmitted byte? Is it somehow sync...

WKowo by Associate II
  • 1426 Views
  • 2 replies
  • 0 kudos

Please correct my function ?

Dear Member,I'm confused between pointer and array,Please correct me :void sim7600_modem(char *SIM_TxBuffer){   printf("sim7600_modem ATI\r\n");   //Clear buffer   HAL_UART_Transmit_IT(&huart1,(uint8_t*)&aTxBuffer4, sizeof(aTxBuffer4));   HAL_Delay(5...

Wrong data on I2C 2 ?

Dear Members,I got a wrong data on I2C 2 for LCD, the first time it was ok, after a while it becomes like in the photo, what do you think the cause of it ?I have put a pull up resistor for it 10K, and the speed is 100KHz,I2C1 for Accelerometer and te...

0690X000009ZXuZQAW.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.