STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO interrupt keep systick interrupt from occuring?

Hi, Im senior engineer using stm32, maybe, not newbee.I know that Higher interrupt priority can occur when mcu still process lower interrupt.Higher interrupt , i mean, lower priority value in nvic register.but just now, I found gpio interrupt can dis...

jd kim by Associate II
  • 2381 Views
  • 4 replies
  • 0 kudos

ADC Sampling rate understanding

I do not understand the difference between the different sampling rates (cycles3 - cycle480). I know it is related to the time given for the ADC capacitor. I also realise that more time should mean more stable reading. I ran some quick tests and I f...

SSudh.12 by Associate
  • 1888 Views
  • 1 replies
  • 0 kudos

Output of STM32F100RB DiscoveryVL board when connected to 3v3 converter only shows from 2.58 to 3.19 volts on the input and alway 5v on the output of converter.

I have a Value Line Discovery board - STM32F100RB and three of the outputs are connected to a 3v3 converter to get a 5v output. I have tried another controller board with 3v3 outputs to drive the convertor board and I get a clean signal. (Either 0 or...

Dan in WY by Associate III
  • 1227 Views
  • 1 replies
  • 0 kudos

Can't erase flash on STM32407VG Discovery

I'm a bit lost by this one. I can write to the flash but cannot erase a sector. I can erase sectors with the ST-Link Utility. The result codes at every step indicate success, but the flash is not actually erased. I am using the Standard Peripheral Li...

Resolved! Sending data to SPI via DMA

I'm using STM32F429 and trying to use HAL library to communicate to SPI slave via DMA channel. I'd like to ask how is resolved problem with for example sending data to SPI via DMA? Is there any kind of synchronization between SPI and DMA to disallow...

WKowo by Associate II
  • 2024 Views
  • 3 replies
  • 0 kudos

STM32 Timer OPM question

Hello,is there any way to achieve this timer OPM behavior?Arm timer ->Output is inactiveStart timer-> Output gets avtiveCompare register triggers -> Output gets inactiveARR triggers: Timer stops _and_ Output stays inactiveAt the moment, I force the O...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.