STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! File-system for NOR flash

Hello,I am struggling with integration of filesystem on external nor.I've been trying both littlefs, and spiffs. Both, with no success yet.Is there any suggestion from ST for filesystem example on external nor flash ?Thank you!ranran

ranran by Senior II
  • 3566 Views
  • 3 replies
  • 0 kudos

Data Splitting??

Hi,I am using stm32h753, in my design. I am using SAI Peripheral for audio(TAS2770 Ic) with internal synchronization method. In receiving mode ,my configuration of slot is slot 0 | slot1. In transmitting mode, configuration of slot is SAI_SLOTACTIVE_...

Vel by Associate III
  • 851 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G0 DAC ADC TIM2

Using TIM2_TRGO to trigger DAC. That works.​Now want same TIM2_TRGO also to trigger ADC.Is that possible ?Regards Juergen

JuM by Senior
  • 1992 Views
  • 3 replies
  • 0 kudos

mpu6050 returns zero, I2C stm32f103

I am working with MPU6050 and STM32f103VE as master. When I wake up the sensor and ask for information it returns 3 bytes of zeroes and the protocol stops working. I only send the communication Part of my code to be more specific:void I2C_interface(v...

Delay in microseconds for stm32l0 cortex m0+

I Wanted to generate the microsecond delay function, I have tried below functions but these are not working, It will be good if someone knows the delay function.static inline void delay_us( uint32_t micros){   micros *= (SystemCoreClock / 1000000) / ...

Resolved! Cannot connect to STM32H753I_EVAL2 board anymore

I know it sounds like a dumb question but I cannot connect anymore to my STM32H753I_EVAL2 (that I've been using extensively for months). I checked the driver in Windows Peripheral Manager. It is properly installed and it shows the same driver DLL as ...

Gpeti by Senior II
  • 935 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.