2019-09-18 3:39 AM
I am working with MPU6050 and STM32f103VE as master. When I wake up the sensor and ask for information it returns 3 bytes of zeroes and the protocol stops working. I only send the communication Part of my code to be more specific:
void I2C_interface(void){
I2C1->CR1 |=I2C_CR1_START; //Generating Start condition
while(!(I2C1->SR1 & I2C_SR1_SB)); //making sure the communication has started
(void)I2C1->SR1;
I2C1->DR=(0x68<<1); //clearing SB and writing MPU address in "writing" mode
while(!(I2C1->SR1 & I2C_SR1_ADDR)){}; //waiting for the address to be sent
(void)I2C1->SR1;
(void)I2C1->SR2; //clearing ADDR bit
I2C1->DR=(0x6B); // addressing MPU internal power management register
while(!(I2C1->SR1 & I2C_SR1_TXE)){}; //waiting for bye to be sent
(void)I2C1->SR1;
I2C1->DR=(0<<6)|(0<<5); // clearing sleep mode bit
while(!(I2C1->SR1 & I2C_SR1_BTF)){};
I2C1->CR1 |=I2C_CR1_STOP; //generating stop condition
while((I2C1->CR1 & I2C_CR1_STOP ));
// **** second part ****
I2C1->CR1 |=I2C_CR1_START; //generating start condintion
while(!(I2C1->SR1 & I2C_SR1_SB)); //making sure the communication has started
(void)I2C1->SR1;
I2C1->DR=(0x68<<1); //sending address in "writing mode"
while(!(I2C1->SR1 & I2C_SR1_ADDR)){}; //waiting for the address to be sent
(void)I2C1->SR1;
(void)I2C1->SR2;//clearing ADDR
I2C1->DR=(0x71);//sending address of internal register
while(!(I2C1->SR1 & I2C_SR1_BTF)){}; //waiting for the address to be sent
(void)I2C1->SR1;
(void)I2C1->DR;
I2C1->CR1 |=I2C_CR1_START; //generating start condition to read data
while(!(I2C1->SR1 & I2C_SR1_SB)); //making sure the communication has started
(void)I2C1->SR1;
I2C1->DR=((0x68<<1)|(0x01)); //sending MPU address this time in "read" mode
while(!(I2C1->SR1 & I2C_SR1_ADDR)){};
(void)I2C1->SR1;
(void)I2C1->SR2;
I2C1->CR1 |=I2C_CR1_ACK; //enabling ack bit
while(!(I2C1->SR1 & I2C_SR1_BTF)){}; //Waiting for MPU to send data of the requested register
I2C1->SR1;
(void)I2C1->DR; //clearing BTF
while((I2C1->SR1 & I2C_SR1_BTF)){};
}
The first part of the code is responsible for clearing register
0x6B
in order to wake MPU up. The second part reads the requested register information. And here is what I get from the communication.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.