STM32H743 VOS RANGE WITH EXTERNAL REGULATOR
Dear All,What is VOS range while using external regulator for STM32H743 ?Thanks,
Ask questions, find answers, and share insights on STM32 products and their technical features.
Dear All,What is VOS range while using external regulator for STM32H743 ?Thanks,
In our design we use QUAD SPI for memory interfacing, can we use QUAD SPI separately for two different memories.
From the datasheet diagram (attached), it seems like the DMA has access to all of above. However, it is not clear whether it is really possible to DMA data to / from those and how I should do it and I've seen negative response to similar chips, so I ...
Hi all,I am trying to design PID controller to monitor LED temperature Control Variable: Parameter that adjust the LED brightnessProcess variable: LED temperature (measuring it with sensor) I am looking for some tips to tune my PID parameters as well...
I am trying to control the amplitude of a triangle wave, while the frequency of the waveform should always be 1kHz. Is this possible to do?The reference manual says that I can control the amplitude of the signal using the register DAC-> DHRx. Further...
I'm using the STM32F303xx MCU in an application with a 24.576MHz crystal. The MCU is powered from 3.3v. I am currently clocking the processor at 3x 24.576MHZ, or just slightly under 74MHz. I realize this is above the rated maximum processor clock ...
Hi. I bought stm32f469i and Nucleo-h745 boards. H745 connects to STLink no problem. But the F469 discovery board doesn’t connect. I tried installing reinstalling drivers, connecting to other computer nothing worked. I couldn’t find another cable that...
I have the code working fine with the 1byte, 2bytes and 4bytes programming, reading and writing. But when I use the 8Bytes (double - word), It is always trapped in a hard fault handler. Any help?
I use the MCO pin to test my clock configuration on a STM32F072RBT6 board. While I'm debugging with a ST-Link/V2 adapter the MCO output shows 24 MHz instead of the expected 48 MHz.Using the exact same software (no changes in clock configuration) and ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.