STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NACK when reading a register through I2C communication

Posted on July 07, 2018 at 04:41Hi, I'm having trouble reading a register in a slave through I2C communication. Slave: bq25895 http://www.ti.com/lit/ds/symlink/bq25895.pdfIn main:while (1){   HAL_StatusTypeDef status = HAL_OK;    uint16_t return_val...

STM32L432R DAC1 out2 configuration

the DAC1 out1 working fine as programmed bt DAC1 out2 is not. Is it due to bridge18 A4 to D4, should I remove bridge. I try setup D4 as Analog and Digital IN and does not helped. Is STN32L$#@RC damaged on out2?

CJaro by Associate
  • 882 Views
  • 0 replies
  • 0 kudos

ADC not working on STM32H750VB

Hi,I have a single adc channel where i read the input values through polling, but it always outputs the max value or almost max value (~ 65280+) as long the input voltage value is greater than zero (v0.5+ ). i configured VREF+ to internal voltage ref...

'F427 ADC channel 16 (temperature sensor)

The 'F427 (437/429/439 "BigManta") is pretty much completely backward compatible, meaning, that a reasonably well written 'F405/407 program (i.e. which does not touch the bits reserved in 'F405/407) binary will run unmodified in the 'F427. There are ...

STM32H7 - start a RAM image

Hi all,I would like to boot a RAM image. A simple bootloader in flash reads in a linear binary from external spi flash. The RAM image works fine if I load it directly to (AXI)RAM (with JTAG).But when loaded by the boot loader, it does not work (loops...

Microman by Associate III
  • 869 Views
  • 1 replies
  • 0 kudos

Init RCC on a STM32F3 (SOLVED)

------------------------------------------------------------------The init of RCC was correct. The SystemCoreClock variable dont reflect the new frecuency changes still "SystemCoreClockUpdate" is called.-----------------------------------------------...

JAlca by Senior
  • 1102 Views
  • 0 replies
  • 0 kudos

Why don't you make a better debugger than STM-STUDIO?

Some time ago I tried your STM-STUDIO: I found it very rough and can only be used for laboratory debugging.Why don't you plan to build a more flexible debugger that can then be used by the end customer to view internal data or change parameters?If yo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.