2019-12-09 6:15 AM
I am using ADC1 and ADC2 of STM32F446RE, which are operated under the following conditions;
I can correctly read the converted values through ADC1->DR and ADC2->DR.
However, I can not read the correct converted values through ADC->CDR.
(Each converted value is always zero...)
According to the manual, the contents of ADC-CDR contains the data of ADC1->DR and ADC2->DR in dual ADC mode.
What key points am I missing? or ...
2019-12-09 9:53 AM
This appears to work only is ADC_CCR.DMA is nonzero. I know, this is not documented. Also, ADC_CSR.EOCx bits are cleared by the CDR read - this is understandable, but not documented either.
JW
PS. Change your username to a normal nick.
@Vincent Onde @Imen DAHMEN
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.