STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Why is CMSIS/DSP arm_fir_f32() using more than one clock cycle per tap? (not using VLMA instruction)

I am currently performing timing and performance measurements for the CMSIS/DSP FIR filter functions on an STM32F412. I toggle a GPIO before and after executing the arm_fir_f32() function and record the signal on a scope.My results are:Details: Sampl...

0690X00000BuVYoQAN.png
Mnemocron by Associate III
  • 3121 Views
  • 1 replies
  • 0 kudos

STM32F4 - Problem with UART Receiver

HelloI'm trying to communicate STM32F411RE (NUCEO board) with SIM800L module through the USART interface.I made USART initialization by HAL driver but I want to communicate manually by referring to the registers directly.USART Initialization:void uar...

0690X00000AtT5yQAF.png 0690X00000AtT71QAF.png 0690X00000AtT76QAF.png
MW9501 by Associate
  • 1226 Views
  • 1 replies
  • 0 kudos

hard fault error while debugging UlinkPlus debugger

I tried debugging STM32 chip using ULinkPlus debugger. When I try to debug for the first time, no issues. For the next time, If theDebug configuration is "Erase sectors", When I try to debug STM32 chip with UlinkPlus Debugger, it throws hard fault e...

Iswarya by Associate II
  • 1017 Views
  • 1 replies
  • 0 kudos

communication dual core 5 (STM32H747)

Quelqu'un parle français ici ? Je suis entrain d'utiliser le stm32h747, je suis une vrai novice. Je dois faire communiquer les deux coeurs, mais j'y arrive pas. alors svp pouvez m'expliqer comment ça marche? ou me montrer un exemple de programme?Mer...

Esam.1 by Associate
  • 739 Views
  • 0 replies
  • 0 kudos

lan8720 soft reset problem

Hi,I have a lan8720 phy board and I use this board with stm32h7 .I didn't change lan8742 source and header codes .Lan8720 board isn't make soft reset .

Bilge by Associate III
  • 1114 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F107 I2C SCL stays low

Hello, I'm working on a project, where the Master (STM32F107) have to communicate with a few slaves (ATxmega) via I2C. Most of the time it works fine. But sometimes the SCL line is going low and stays low. First i thought it's a Slave issue (because ...

user 143 by Associate III
  • 5997 Views
  • 4 replies
  • 0 kudos

48MHz clock source selection, not necessarily 48MHz?

I have (another) dumb question... but I learn so much from my dumb questions, so bear with me.On our STM32F7, we are using a couple of peripherals that use the PLL48CLK. I see from [RM0410, Figure 13 page 153/1954] that this is selectable as the out...

garbage value with sprintf

hi everyone,Can someone tell me if sprintf is ok in Keil? Tera term prints garbage value.2 days ago I tried sprintf and it didn't work, I tried a simple declaration of a string and it worked.what's the problem?

0690X00000AtWZDQA3.png 0690X00000AtWZSQA3.png 0690X00000AtWZXQA3.png
idrissmc by Associate III
  • 1451 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.