STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer don't work when set ARR=0

HiWhen I want timer count (CNT register) until ​5000 for overflow , Set ARR = 5000-1; now I want timer count until 1 So I have to set value ARR = 1_1 (ARR = 0) But When Set ARR = 0 timer don't work and don't have interrupt. Why??​​how to set ARR Fo...

mkari by Associate III
  • 5393 Views
  • 7 replies
  • 1 kudos

Make 32bit timer by 2 16 bit timer

HiI make a 32 bit timer by to 16 bit timer3(master) & timer4(slave)Now I want my timer count antil 150000 (for example)​How to get 150000 in two TIM3->ARR & TIM4->ARR register??Does it have a special formula?this number (150000) isn't ​fixed.I have a...

mkari by Associate III
  • 3609 Views
  • 10 replies
  • 1 kudos

UART error under reception on TSM32L051C8.

Hello.I am trying to change an old source code where a new UART port is implemented using pins PA2 and PA3 (UART2). When I run the old code with changes made for UART2 I've got communication errors Parity, noise, frame and overrun error. The huart->E...

BLilj.1 by Associate
  • 758 Views
  • 0 replies
  • 0 kudos

Ram disk error : FR_NO_FILESYSTEM

Following me prev. question:I am using STM32F429zi boardBut found a RAM_DISK example for 9i boardI ran with / without RTOSIn both cases :all these word fine (return woth OK :(FATFS_LinkDriver, f_mount, f_mkfs, But when I call f_open I get FR_NO_FILES...

ECrom.1 by Associate III
  • 858 Views
  • 0 replies
  • 0 kudos

All UARTs are functional with DMA except for LPUART

Hello,I manage to operate all UART/USART DMA's except for LPUART.For some reason, only with LPUART, I fail to start DMA transaction.Is it because it's request are from DMA2 instead of DMA1 (all UART's are connceted to DMA1, except for LPUART, which i...

ranran by Senior II
  • 1155 Views
  • 2 replies
  • 0 kudos

Debugging of STM32L072CZ

As I am doing debugging for STM32L072CZ Controller using ST-Link/V2 debugger with Software Keil and AC6. As I am getting No target device found. So suggest me how to solve thr error.

STM32H747 ADC Internal Reference usage and stability

HelloI am new to STM32 family and currently I was working on STM32H747I-DISCO board with HAL device support. Is it possible to change the ADC reference from external Vref+ to internal Vref ? if possible how to configure? why because there is no param...

Kranthi by Associate II
  • 3492 Views
  • 9 replies
  • 0 kudos

UART receive data problem

Hi,I am using stm32f103 mcu for UART data transmit and receive. I am using UART interrupt for both receiving and transmitting. Sometimes received data takes a different value than it should be. This occurs when i send some data from stm32 to serial p...

er3481 by Senior
  • 2201 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.