2020-02-13 4:44 AM
I am using STM32F103C8T6(Blue Pill) with STM32IDE.
> I am trying to learn external Interrupt. So as a reference i am using 3 main thing.
# Reference Manual
# DataSheat
# Cortex™-M3 Devices Generic User Guide
> I wrote a code for this. I made changes into registers.
Here is my Github link.
> When i am trying to set NVIC_ISER0 Register it set my desired bit but NVIC_ICER0 Register also set same bit. Which is Strange for me and I don't Know why is it happening ?
# If NVIC_ISER0 bit set means Interrupt at that IRQ is Enable.
# if NVIC_ICER0 bit set means Interrupt at that IRQ is Disable.
> When I am giving Interrupt Then the Pending bit of EXTI->PR register and I also saw that NVIC_ISPR0 Bit(1<<IRQ) also set when i give interrupt. But Still I am not getting any call for my ISR.
> At last my ISR is not called and Control goes to unknown location.
2020-02-13 6:23 AM
> EXTI_IRQHandler()
There is no such thing. Look into the startup code (startup_stm32xxxx.s -- e.g. https://github.com/STMicroelectronics/stm32f1xx_hal_driver if you use gcc-based compiler), there you see the vectors table, you should use only names from that.
JW
2020-02-13 6:31 AM
>> EXTI_IRQHandler()
> There is no such thing.
And, interrupt handlers do not have any arguments either.
2020-02-13 8:35 AM
Thanks @Community member and @Ozone You saw my code.
> EXIT_IRQHandler() is define by me where I am setting NVIC interrupt Register.
> I saw in Startup file and get useful ISR which is weak So I write by my Self in main.
>> For your Kind Information that My code is running and I am getting Interrupt as Required.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.