STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! No CAN Communication on STM32H723ZG-E01 (A230801274)

Dear STMicroelectronics Support, I am working with the STM32H723ZG-E01 board (Serial: A230801274) and encountering an issue where CAN communication is not functioning as expected. Based on the documentation, I have configured the FDCAN1 interface to ...

mani9989 by Associate III
  • 13242 Views
  • 20 replies
  • 6 kudos

STM32H7 Max UART Baudrate

Posted on November 24, 2017 at 16:15I tried to figure out the specification of the max. UART baudrate for the SM32H7 series (@ 400MHz system clock).The data sheet says 12.5 MBit.Does this apply to all UART ports or only selected ones?I need 8 MBits ...

Resolved! STM32F723x USB HS CoreReset Issue

Hello, for the last couple of days I've been trying to set up my STM32F723ZET6 project as a USB HS CDC device with internal PHY.My code gets stuck in this loop do { count++; if (count > HAL_USB_TIMEOUT) { return HAL_TIMEOUT; ...

BRapo1_0-1747726756614.png BRapo1_1-1747726855418.png BRapo1_2-1747726886964.png
BRapo.1 by Associate II
  • 2142 Views
  • 5 replies
  • 3 kudos

STM32 Boot mode Pin functionality

Hi,I’m currently working with the STM32G491RE MCU and have encountered an issue related to GPIO pin PB6.In our normal user application, PB6 is configured as a push-pull output. However, we would like to understand its behavior when the device enters ...

Resolved! STM32H7 FMC - SDRAM byte and bit swapping

HiI am working on a project with an STM32H743 and a 32-bit SDRAMThe FMC signals are quite randomly scattered across the package and this makes layout quite convoluted and difficult. I'd like to swap byte-lanes and individual bits within each byte, fo...

JF999 by Associate
  • 1484 Views
  • 2 replies
  • 0 kudos

Resolved! does stm32f103c6tx support external loopback?

I wrote a code for this microcontroller to test the CAN protocol, and it worked successfully in loopback test mode—data was transmitted and received correctly without using any external CAN transceiver. Then, I switched the CAN mode from loopback to ...

ssharrafi by Associate II
  • 1811 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.