STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L475 Multiple wake up interrupts for stop2 mode.

Hi Community,I am working on deveoping applications on STM32 IoT Doscovery kit. I am interested in the lowe power design aspects as far as the sensor reading is concerned. This is my first time working with sleep modes / reducing power consumption. C...

How to know the MCU address for its use as an I2C slave ?

Hi guys, I would like to connect two different MCU to each other through I2C. One MCU would be the master, and the other one the slave. How can I find the I2C addresses of these devices ?I found the device ID in the reference manuals : 0x411 for STM3...

HHUET.1 by Associate II
  • 1479 Views
  • 1 replies
  • 0 kudos

Resolved! Load capacitance (AN2867)

I am working in small startup in Bangalore. I had designed the board using the STM32F103R8T6 controller now i am facing oscillator issue, oscillator is not working as i expected. thereafter i googled it for oscillator design guide and i found AN2867....

Bhat by Associate II
  • 11820 Views
  • 6 replies
  • 0 kudos

ADC front end design to remove high frequency noise

Hi everyoneI am working with STM32F429Zi microcontroller on a customized board. I am acquiring the signal shown below (oscilloscope screenshot) with ADC3 at a sampling rate of 300ksps. The input signal is a 10kHz sinusoidal waveform superimposed on a...

0690X00000DXP25QAH.png 0690X00000DXP2AQAX.png 0690X00000DXP2FQAX.png
ADITI by Associate II
  • 4090 Views
  • 4 replies
  • 0 kudos

Should I set HAL_DMA_STATE_READY in circular mode?

Hi,I'm implementing a circular buffer for UART transmit via DMA on an STM32L4 device.I've got a callback that updates the read pointer and calls another HAL_UART_Transmit_DMA if it's still not equal to the write pointer.This callback is called by:HAL...

Stijn1 by Associate II
  • 2131 Views
  • 4 replies
  • 0 kudos

Will resetting the RTC (Real Time Clock) module frequently destroy the microcontroller due to excessive writes to non-volatile storage?

I am in the process of understanding the internals of the RTC (Real Time Clock) inside the STM32F446 microcontroller. I have already written some code and released it and now I'm afraid that the code might damage the microcontroller in the long run. ...

arnold_w by Senior II
  • 728 Views
  • 0 replies
  • 0 kudos

How to increase SPI display (ili9341) draw speed?

How to fill the screen with one color without seeing the draw pattern from top to bottom?All I want is to make screen instantly change color. I understand that drawing bitmap might be slow, but I want just one color.Is there a way to reduce display c...

JBond.1 by Senior II
  • 3276 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.