STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

the RM0090 reference manual for 2014 ,in the description of the “Chip Select togglest�? different from RM00990 reference manual for 2018,why?

the RM0090 reference manual for 2014 ,in the description of the “Chip Select togglest�? different from RM00990 reference manual for 2018,which one is correct?The results of our tests are consistent with reference manual for 2014,Is it wrong in RM0099...

0690X0000087VffQAE.bmp 0690X0000087VfaQAE.bmp
cxiao.6 by Associate II
  • 4010 Views
  • 8 replies
  • 0 kudos

I have a question,when changed cpu from stmf407 to stm32f427 .sometimes, read a wrong data from extern sram access by FMC ,it's happend in most of the cases in interrupt ,someone have the same problem?

my English is poor,In the same program ,cpu 407 do not have this problem,only happened in 427​,somtimes.It's like 2.3.4 Corruption of data read from the FMC. in <Errata sheet - STM32F42xx and STM32F43xx - STM32F427/437 and STM32F429/439 line limitati...

cxiao.6 by Associate II
  • 2478 Views
  • 4 replies
  • 0 kudos

printf function call causes hard fault

Hi all,I am working on a STM32F103VEtx MCU. In my firmware I have redirected the printf function to a UART for debugging purposes. When I start running the code, the printf function causes the hard fault handler to hit. Please see the call stack att...

0690X00000DXN5RQAX.png

Effect of timer CCR not in range 0<CCR<ARR

DMA requests are still generated if the CCR is outside the auto-reload rangeThe DMA request is is generated when CNT reaches 0 rather than being disabled.Processor is a STM32H750is this a bug or a feature - it should be documented anyway

pbayton9 by Associate III
  • 1649 Views
  • 2 replies
  • 0 kudos

Trying to go into, then out of sleep mode. Two problems.

Problem 1)  current draw does not change after entering sleep mode.Problem 2)  not sure if program should resume where it stopped or from the beginning of main. Also any difference between waking by NRST or by A0 set to PWR_WKUP0?Mcu is 'H747 operati...

PAngl.14 by Associate II
  • 1412 Views
  • 2 replies
  • 0 kudos

Please order with newest first as default!

Hello,https://www.st.com/en/microcontrollers-microprocessors.html#resourcestarts with some unknow order. Clicking on the "Latest update" results in the oldest on top. Only with a second click, the newest entries git first. These resources are mostly ...

[TIM] how to read current TIxF state

I want to know the current level of the channel-input filter's output, marked as TIxF on the diagrams and in narrative.I know I could read the respective pin, but that's not the same - it misses the filtering aspect, i.e. a single read might inadvert...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.