STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32F4 and CAN bus

hi there,i am working on a project and i have to connect two stm32F4 boards via CAN bus. i ve been looking on the internet for days now but i can't manage to find a circuit nor a code to that. i desprately need your help. thank u.

SGUIG.1 by Associate II
  • 698 Views
  • 0 replies
  • 0 kudos

Details on STM32G474 DMAMUX?

The information in the reference manual (RM0440) is very limited. There is an app note: "AN5224 DMAMUX description" but it says it only covers STM32H7, STM32G0, STM32L4+ and STM32WB series.Also, if you search the resources for the STM32G474 this appl...

IAP issue with STM32L152RE

I am using stm32l152re. What I'm doing right now is uploading IAP (in application programming) to stm32l152re. First, I uploaded successfully through JTAG using the IAR IDE, but the serial communication through uart did not work properly.The procedur...

JChoi.2 by Associate
  • 633 Views
  • 0 replies
  • 1 kudos

Changing Baud Rate results in Framing Errors – STM32F303

I have a GPS module I'm talking to at the default 9600 baud. I then send it a command to change the baud rate up to 115200. After the command is sent, I believe the GPS module is correctly switched over to the new baud rate, since I immediately will ...

SWill.11 by Associate II
  • 2802 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.