STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! *.zip file decompression - STM32F7

Hi all, I just want to decompress a .zip/.7z file store on external flash. Could some one tell me some sort of library work with STM MCUs meet my requirement?Thanks in advance.

Resolved! STM32 memory to memory DMA with Timer

Hi, I am trying to do MemToMem DMA operation on Timer input capture.My code:#define BufferSize 1000 uint16_t BUFFER_DATA[BufferSize];   TIM_HandleTypeDef htim = htim3; DMA_HandleTypeDef hdma = hdma_tim3_ch4_up; uint32_t channel = TIM_CHANNEL_4; uint3...

JBond.1 by Senior II
  • 2149 Views
  • 2 replies
  • 0 kudos

UART in DMA cause MCU crash

hi every one i am trying to receive data with UART in DMA and Normal mode, but after about 10 times that I receive data correctly suddenly MCU stop working I checked every thing but I don't know what's wrong :sad_but_relieved_face: this is my Uart an...

rhaja.1 by Associate II
  • 4412 Views
  • 9 replies
  • 0 kudos

SPI communication between Slave and Master

This is my first post on this QnA section and i hope i would be getting help from the community. What i want to implement is a simple communication between 2 STM32 (both are F1 series in this case) using a SPI. Both the MCU are configured using CubeM...

0693W000000Vys5QAC.png 0693W000000VysAQAS.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.