STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Two single-ended ADC inputs vs differential ADC

Hello,Does STM32F7 support differential or pseudo analog reading?Also Other than that if we read two single ended channels which are connected to a differential pair and then in software we do the common mode rejection does it have the same performan...

MMehr.1 by Associate
  • 4784 Views
  • 5 replies
  • 0 kudos

Resolved! How to use internal clock on STM32G070CBT6

Hi,I'm going to use STM32G070CBT6-LQFP48 MCU in my project.I need to use the INTERNAL CLOCK.Is there any application that explains how to do it or how to configure the dedicated pins?Thanks in advance for your support.Fab

FLM.1 by Associate II
  • 3043 Views
  • 5 replies
  • 0 kudos

Resolved! Problem with a Timer DMA Burst mode

NUCLEO-F103RB with STM32F103RBI want to use the DMA in a burst mode to write data from buffer in RAM to the TIM1_CCR1,2,3,4? that are in PWM mode. DMA burst transaction is requested on the TIM1 Update (UEV). Number of transactions in Burst mode is se...

0693W000000WWxdQAG.png

Resolved! Problem with Updating RTC_TR and RTC_DR registers in STM32F098:

I want to use RTC module in STM32. Eventhough i try to update the date and time registers, their values are not updated. I have given my code. I would be thankful, if someone can point out what is the wrong with my procedure. uint32_t _Time_Tens=0,_T...

SFons.1 by Associate II
  • 2281 Views
  • 3 replies
  • 1 kudos

STM32L475 Touch Sense not changing status from BUSY

Hello! I'm trying to use a custom PCB STM32L475 with the touch sensing library based on the 1 touch example there is available for the L4xx.I've configured the PC8 pin as TSC_G4_IO3 (as sampling pin) and both PC6 and PC7 as TSC_G4_IO1 and TSC_G4_IO2 ...

NFerr.1 by Associate II
  • 1349 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.