2020-02-12 1:15 AM
I need to have ADC1 and ADC2 run sumultaneously. Each ADC has 2 injected channels. I want to start the ADC once and then have it constantly run converting the 4 injected channels, putting the result in the 4 associated JDR registers and raising a flag in the ADC conversion complete interrupt to tell my main program that data is available for me to read from the 4 JDR registers.
Is that possible, if so can someone kindly provide example code?
The ADC on this uC is so complicated, I can not make heads or tails of anything.
2020-05-05 4:39 AM
Hello @ATo
Please refer to Injected simultaneous mode in STM32H7 reference manuel RM0433 Rev 7.
Best regards
Bouraoui
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.