STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Accessing Timer OC register for DMA transfer.

Hi All,I'm using a STM32F302R8 and want to transfer timer 2 capture/compare values to memory using DMA. What source address do I use for the TIM2 OC register? I'm calling HAL_DMA_Start() to do this and need the source address of TIM2->OR.Thanks,

BTrem.1 by Senior II
  • 1209 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H753 vs STM32H743: Can I substitute?

I need to get some PCBs made by JLC but they are continually out of stock of the STM32H743IIT6 which is my target processor. They do however have the STM32H753IIT6. Is there any reason I can't substitute these to run identical firmware?Thanks

PMath.4 by Senior III
  • 3817 Views
  • 8 replies
  • 0 kudos

Resolved! Questions about this circuit and a solution

Hi,Master:​​Platform: STM32F301K8U​As shown below in Figure 1, PA7 (MCU_14) is a video signal (As shown below in Figure 2), which contains the line sync signal (A area in Figure 2, fixed frequency, there may be noise)​and the field sync signal(B area...

0693W000000Wvs9QAC.jpg 0693W000000WvlxQAC.jpg 0693W000000WvuPQAS.jpg
Lyu.1 by Senior
  • 2503 Views
  • 7 replies
  • 0 kudos

STM32H750VB SPI Slave MISO last bit returns low to early

Hi there,I am using the STM32H750VB as an SPI Slave in Interrupt mode and it is working but I am not happy with what I see with my analyzer.SPI is working with Idle-Clock Low and aquiring data at leading edge. LSB first.That's all how it should be bu...

TAlbr by Associate
  • 2176 Views
  • 3 replies
  • 0 kudos

STM32F103CBT TIM4 PWM with DMA results in Hard Fault

Hi, Beginner question: Over the last few days I've tried to generate a PWM signal with a STM32F103CBT on Pin 46 (PB9) with a variable pulse width, but apart from generating a signal with a fixed Duty Cycle at the desired frequency (800kHz - I want to...

TSchr.1 by Associate II
  • 3828 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.