STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What are TIMx TIx[1..15] input signals?

TIM1 section figures 55 and 79 in G0 reference manual RM0454 Rev2 refer to TI2[1..15] as selectable sources for TI2 signal (see also TI2SEL register bits). It appears that TI2[0] is the TIM1_CH2 pin, but what are the sources for the TI2[1..15] signa...

GPope.1 by Associate
  • 1554 Views
  • 2 replies
  • 0 kudos

STM32F745vg Hardfault handler.

sir,Am uisng STM32F745vg controller for stepper motor controlling through a driver.while running program am getting hard fault handler .can you provide why hardfault interrupt occure.what is the solution for hard fault handler.

steja by Associate II
  • 1648 Views
  • 2 replies
  • 0 kudos

Resolved! Nucleo F401RE Usart Tx Blink Led

I have Nucleo F401RE board.I want to Turn On Led When Usart Tx pin high and Turn Off When Usart Tx pin is low./* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ uint8_t data_tx[5] = {0x41 , 0x42 ,...

AN5094 comments

https://community.st.com/s/question/0D50X0000CBn2icSQB/nucleog431kb-help-with-dma-gpio-outputJW

0693W000000WeNdQAK.png

Send UART hex command

HiI'm trying use DFR0534 with STM32f446.This module read uart command hex.Ex. Command AA 07 02 00 08 BBIm trying send like thischar play[6] = {0xAA, 0x07, 0x02, 0x00, 0x08, 0xBB}; HAL_UART_Transmit_IT(&huart4, play, 6);But in uart monitor recive diff...

Mkal.1 by Associate
  • 4110 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F446RE Can't use Pins PA2, PA3 as Input

Hi,I am trying to use the PA2 and PA3 Pins among others as Inputs with Pullups. The configuration is correct, since I am comparing what is in the GPIO Registers for Port A with another input pin PA8 which works fine. I have seen that the same pins us...

FLewz.1 by Associate III
  • 5341 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.