STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32F412 SPI interrupt full duplex slave.

Hi I am working on stm32F4 on spi communication. I am using stm32F4 as slave module and i have other qualcomm board as master module. as in master module there are 5 pins as MOSI,MISO,SCK,CS,INTR. when I am generating the code for stm32f4 using cubem...

Kpand.1 by Associate II
  • 3918 Views
  • 8 replies
  • 0 kudos

STM32F4 SPI slave TX/RX error: how to reset SPI?

Hi, I'm using an STM32F413RG MCU as SPI full-duplex slave, initialization is done in Cube. Every 500ms the master activate the SPI_CLK (1MHz) and the MCU outputs 16 bytes of data while receiving other 16 bytes from the master (using HAL_SPI_TransmitR...

dvd by Associate II
  • 2375 Views
  • 2 replies
  • 0 kudos

F767 TIM12 PWM HAL not working

Hi,I tried really hard to get the TIM12 working, but I had absolutely no success... I already do PWM on TIM1 and TIM4. So I tried with same settings to setup TIM12, but it does not work. The question now is: Why?What do I use?STM32CubeIDE 1.3.0I set ...

PKlar.1 by Associate II
  • 5616 Views
  • 11 replies
  • 1 kudos

Resolved! Using RTC on STM32l4 as a fail safe monthly wake up?

Wondering if the STM32l4 RTC could be used to wake the processor from standby mode after 1 month.Powered by the LSI, would the time drift beyond usability? Ie. It does not matter if the device wakes up 30 days or 31 days later. Just as long as its in...

Resolved! STACK and HEAP size

Hello everyone In Keil Projects we are able to change Stack_Size and Heap_Size in "startup_stm32f746xx.s" file like this :Stack_Size      EQU    0x400Heap_Size     EQU    0x200BUT in IAR projects there isn't such code line in the startup file related...

MSm by Associate II
  • 4341 Views
  • 2 replies
  • 0 kudos

Weird triggering of SPI interruption on STM32H743

I'm facing a weird situation. I'm using SPI simplex receive-only mode on a Slave STM32H743. It has been working fine for a while. Until now I was enabling only the RXP interruption. The SPI1 interrupt was triggered as expected.Now I enabled also EOTI...

0693W000001q7U1QAI.jpg
Gpeti by Senior II
  • 1670 Views
  • 5 replies
  • 0 kudos

Resolved! Frequency range of LSI for STM32L072CB

Hello,according to the datasheet of STM32L072CB there is a margin of controllers which have at 26kHz@Xx°C or 56kHz@Xx°C (first row of table)?So in total there is a production margin (26kHz to 56kHz) and additionally a temperature drift during run tim...

0693W000001q5y4QAA.png

STM32H743ZI CAN not working

I am trying to use the STM32H743I-EVAL FDCAN_Com_IT example code to run CAN on STM32H743ZIT6. I am trying to transmit at regular intervals. When I look the signals on a scope, the TXD goes low for just a bit interval and then remains high. Here is m...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.