2020-06-05 7:54 AM
Hello everyone
In Keil Projects we are able to change Stack_Size and Heap_Size in "startup_stm32f746xx.s" file like this :
Stack_Size EQU 0x400
Heap_Size EQU 0x200
BUT in IAR projects there isn't such code line in the startup file related to the project. how and where can we change stack and heap size in IAR projects?
Regards
Mohsen
Solved! Go to Solution.
2020-06-05 8:52 AM
Hi MSm,
A clean way to do that is to go to: Project --> Options --> Linker --> Click the 'Edit' button under stm32f746xx.icf file like attached --> then go to Stack/Heap sizes.
Or, you can do this directly from the .icf file :
/*-Sizes-*/
define symbol __ICFEDIT_size_cstack__ = 0x400;
define symbol __ICFEDIT_size_heap__ = 0x200;
/**** End of ICF editor section. ###ICF###*/The first method is the one we recommend.
Best Regards,
Ons.
2020-06-05 8:52 AM
Hi MSm,
A clean way to do that is to go to: Project --> Options --> Linker --> Click the 'Edit' button under stm32f746xx.icf file like attached --> then go to Stack/Heap sizes.
Or, you can do this directly from the .icf file :
/*-Sizes-*/
define symbol __ICFEDIT_size_cstack__ = 0x400;
define symbol __ICFEDIT_size_heap__ = 0x200;
/**** End of ICF editor section. ###ICF###*/The first method is the one we recommend.
Best Regards,
Ons.
2020-06-05 11:01 AM
Thanks a lot ons for your complete reply.
Regards
Mohsen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.