STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is this a normal level of noise to see for I2S with DMA?

I'm getting a lot of noise from my STM32 design, which is just supposed to be direct line-in/out I2S with DMA.I'm feeding in a 440Hz sine wave to my CS5343 A/D converter:And this is the output I'm seeing from my CS4344 D/A converter:If I zoom out a b...

0693W000001qSuUQAU.jpg 0693W000001qSutQAE.jpg 0693W000001qSv8QAE.jpg
NNagy.1 by Senior
  • 2901 Views
  • 5 replies
  • 0 kudos

Stm32F103C8T6 Custom board problems

Hi, i have some rather strange problems with my custom with an STM32F103C8 mcu on it. It is programmed via an Nucleo ST Link v2/1 and it works fine most of the time. I can load some test sketches on it via Platform IO or STM32CubeIde. But after a fe...

0693W000001qYL6QAM.png 0693W000001qYL1QAM.png
TMaie.1 by Associate II
  • 1259 Views
  • 1 replies
  • 0 kudos

Does STM32 has "pulse counter register"?

Hi, anyone know there is a register that can count the pulse directly on STM32H7?I know there is a timer in capture mode, it can generate interrupt when detected edge high or low. But this counter does count the period time only, does not count how m...

Dat Tran by Senior II
  • 754 Views
  • 2 replies
  • 0 kudos

Unity Test Framework Usage

Hi,I wanna use Unity test framework so i cloned from github Unity files. And added my STM32CubeIDE project. And write a simple code for test but i failed when i try build project. Is there anyone know how can i implement unity and use this framework?...

fyazı.1 by Associate II
  • 2019 Views
  • 1 replies
  • 0 kudos

Resolved! Problem reading gpio pins in parallel from multiple eeproms.

Im trying to write to and read data from 10 eeproms in parallel. I first transmit the data in parallel to all the eeproms via spi, I then read data in parallel by first transmitting the address of data stored in the eeprom and then transmitting dummy...

0693W000001qVfmQAE.jpg 0693W000001qVKyQAM.jpg 0693W000001qVKjQAM.png
TSa.1 by Associate II
  • 5691 Views
  • 13 replies
  • 0 kudos

Resolved! Problem in the I2C1 peripherical?

Hi to all!I have an Nucleo-F767ZI board and I noticed a problem, in the I2C1 periperical.I have redirect the I2C1 pins on PB8 and PB9 for comodity and left PA6 and PA7 free and the I2C1 work well.After a couple of days, i have used the PA6 pin as out...

Luca1 by Senior
  • 1733 Views
  • 3 replies
  • 0 kudos

STM32F302K8 I2C weirdness

I have noticed some very strange behavior with the I2C controller. It appears that when it has a slave address match, it sets the ADDR ISR flag and raises an interrupt ( if enabled ). If I have a breakpoint in the interrupt handler, the ISR BUSY fl...

psusi by Associate II
  • 2018 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.