STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! External clock requirement on N6 Family

Hello, I was wondering about the reasons to supply external clocks to the N6 MCU, since it seems that via HSI and LSI there are clocks integrated into the MCU. I am having trouble to understand whether the internal clocks can satisfy my requirements:...

Panda by Associate III
  • 1059 Views
  • 1 replies
  • 1 kudos

stm32H753zi ADC Linearity Tests.

Test procedure.Nucleo-H753zi with "arduino style" shield installed.Hardware includes DAC80501 to generate linear ramp 512 points, than OP amp to scale up and convert SE to Diff.ADC2 runs in Diff mode, channel 3 (PA.6 & PA.7 -> SB 33/ 35 modified),clo...

adc2 diff adc shield 1.jpg H753 ADC Diff Linearity Test.png adc2 diff  calibrated brd.jpg adc2 diff N-4 M-1A0.jpg
MasterT by Lead
  • 1644 Views
  • 2 replies
  • 4 kudos

Resolved! STM32u5g9 usb support

Hello, I have been trying to implement USB support on an STM32u5g9vjt6Q using USBX in standalone mode without success as of yet. I have been referencing this guide (How to implement USBX in standalone mode ) I am trying to use the onboard USB Phy in ...

Screenshot_20250601_160300.png
brohr01 by Associate III
  • 1212 Views
  • 2 replies
  • 0 kudos

STM32H503 code execution performance issue

Hellofor some specific usage I am evaluating possibilities of using CM33 with HCLK 250MHz for maximum code execution performance. To do so I have crafted procedure in assembler and calculated the cycles using ARM reference manual. The code is doing o...

ULPEN - ST please unify nomenclature

In 'G0B1, 'G071 and 'L412 Datasheets, ULPEN is mentioned several times (namely 3 times).It probably corresponds to PWR_CR3.ENB_ULP in case of 'G0x and PWR_CR3.ENULP in case of 'L412/'L422.I did not check if this propagates to newer STM32, too.ST, can...

Square wave FSK issue using PWM ouput

Hi All,I am trying to impliment a frequency shift keying (FSK) routine to represent a each bit of a byte as FSK.My routine is kind of working (see the IRQ for TIM3 below). My FSK is :Bit 0 & Start : 3600Hz Bit 1 & Stop : 1200HzThis ensures that timin...

Screenshot 2025-05-30 124318.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.