STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Overcoming SPI speed limitation on H743- inspiration needed

I'm setting the SPI input clock for the port I'm using at 50MHz to allow SPI speeds up to 25MHz for use with an SD card under SPI. However, this gives a minimum speed of 50MHz/256 = 195KHz and this is too fast for initialising some SD cards. I need t...

PMath.4 by Senior III
  • 2428 Views
  • 4 replies
  • 0 kudos

Flash Sector Resets After Reading for No Apparent Reason

I am writing an application and bootloader to STM32H7.I append some data to the end of the application. My bootloader needs to be able to read this appended data.When my bootloader first writes the application via (erase->write to memory).When the sy...

AAgar.2 by Associate III
  • 1779 Views
  • 2 replies
  • 0 kudos

DMA adds to the time delay of counters

Hello guys I just want to ask why adding a callback is causing additional time delay to counters. In my case I created a periodic pulse using the PeriodElapsedCallback which is in interrupt mode. I toggle the output every 300ms and this is working ...

RSy.1 by Associate III
  • 1991 Views
  • 4 replies
  • 0 kudos

Port A and B disabled when modifying Port D/E on F207ZG

Good afternoon (o;Testing a GPIB code on my Nucleo-F207ZG board...GPIB communication is just fine, which uses PORT D and Port E....Now I added SPI code which reads out temperature from a MAX31855 device....using PA5/6 for SPI and PA4 for chip select...

Davorin by Senior
  • 1880 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.