STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unclear how to setup STM32L4+ clocks for SD card and LPUART

I'm slowly learning how to use the STM32 family starting with the STM32L4R9-Discovery board. I use mostly VisualGDB and have run and modified a variety of UART examples and FATFs/uSD card examples. When I try to put them together so I can log data on...

magene by Senior II
  • 999 Views
  • 1 replies
  • 0 kudos

STM32F429 eMMC driver [SDIO CRC CMD/DATA Error]

I connect STM32F429 with an eMMC NAND via SDIO interface(CLK CMD & DAT0).​This initialization sequence for eMMC should be CMD0, CMD1(wait OCR bit31), CMD2, CMD3, CMD9, .....​The eMMC driver is tested ok on STM32F103 system, including init, read, writ...

ZChen.1 by Associate
  • 1263 Views
  • 0 replies
  • 0 kudos

B-G431B-ESC1 20vdc Max?

Oddly the on board NFETS are rated 60v, why only 20v input? Can we safely go to +48vdc, if not why? Our motor driven FW the voltage does not go above Vbus.Is FOC space vector 7 phase or 5 phase switched? Thanks

BFalcon by Associate II
  • 4374 Views
  • 9 replies
  • 0 kudos

Resolved! How to enable GPIO inputs for INTERRUPT MODE ?

The H745 Datasheet says General-purpose input/outputs : Up to 168 I/O ports with interrupt capabilityYet, every pin I select as GPIO (ex. PORTC.13 (PIN E3)), only lists INPUT or OUPUT options, but no Interrupt mode.If I bypass the Stm32CubeIde 1.3.1'...

bnguy.1 by Associate III
  • 6199 Views
  • 3 replies
  • 2 kudos

Stm32h7 vddldo on non bga packages

Hello, I was looking for an stm32h7 part where I could provide voltage to the internal ldo from a vddldo pin to achieve lower power consumption using an external smps. I'm looking at the h743 lineup but cannot find any package with such exposed pin e...

AAnci.1 by Associate II
  • 1581 Views
  • 1 replies
  • 0 kudos

Resolved! I am usinng STM32H7 nucleo board. I want to generate 20KHz pwm wave. How can I control the resolution (that is a value from 0-10000 that corresponds to 0-100%)?

 So I adjusted the ARR and Prescalar values to adjust the pwm frequency(20KHz). Timer Clock is 200MHzI want to change the resolution in the run time with a function. How can I change it?Changing the ARR value will change the resolution?Thanks in adva...

VRapa by Associate II
  • 2486 Views
  • 4 replies
  • 0 kudos

QUADSPI timings to read, write, erase flash IC

Hello,I've a MT25QL128 IC interfaced with STM32F767 controller on QUADSPI. there is external crystal of 8MHz. I want to check timings req for read, write and erase the flash IC, so that I can write some data into flash. I've referred application note...

AShel.1 by Associate III
  • 2433 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.