STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

speed of execution - pin change seems too slow

I just got a simple program running on my STM32f0301k6. I am running the clock off a 20MHz crystal and the core is running off the PLL x 2 so everything is running at 40MHz. This means one cycle executes in 25nS, but if I write a loop like GPIOB->...

deep_rune by Associate III
  • 5138 Views
  • 13 replies
  • 0 kudos

SAI DMA Data transmit fails on STM32H745 Discovery board

Hi,I have configured DMA and SAI interface as below.void HAL_SAI_MspInit(SAI_HandleTypeDef* hsai){ GPIO_InitTypeDef GPIO_InitStruct;/* SAI2 */  if(hsai->Instance==SAI2_Block_A)  {  /* Peripheral clock enable */  if (SAI2_client == 0)  {    __HAL_RCC_...

NKadi.1 by Associate
  • 1051 Views
  • 0 replies
  • 0 kudos

Changing default parameters of main()

I've got an application where the main() function needs to be non-standard. In older version of GCC this wasn't an issue but the newer versions seem to have changed somethingI need:void main(long long int *c, long long int *b)but GCC is overriding th...

PMath.4 by Senior III
  • 1536 Views
  • 2 replies
  • 0 kudos

Wifi is not connecting with the board B-L475E-IOT01A.

Hello Team,i have flashed B-L475E-IOT01A-WiFi-Bridge-S2LP binary into the B-L475E-IOT01A board and then it asked to enter the input ssid , password and security type. i given all correct value but we are getting the response like "Given SSID not F...

JC.1 by Associate
  • 3237 Views
  • 3 replies
  • 0 kudos

Output Compare Formula [STM32H7]

I'm using TIM5CH3 to toggle an I/O, but AN4013 doesn't list a formula for the Output Compare, so I'm using the Timer Base Generator in Section 2.2: Update_event = TIM_CLK/((PSC + 1)*(ARR + 1)*(RCR + 1))With TIM5 CLK of 60Mhz, Prescaler 60-1, and ARR ...

0693W000001rdUeQAI.png
bnguy.1 by Associate III
  • 2161 Views
  • 4 replies
  • 0 kudos

Cannot connect to Nucleo G031K8 via ST Link

I just bought a STM32G031K8 Nucleo, and when I connect it to ST-Link through Normal mode, the device is not recognized. It hangs, and ST Link throws the error shown in the picture. There should be a problem with Reset because it says it cannot rese...

0693W000001sA32QAE.png 0693W000001sA37QAE.png
xpp07 by Senior
  • 1245 Views
  • 3 replies
  • 0 kudos

Problem initialising RTC on STM32F031 Nucleo-32 board

I am using code generated using CubeMX to configure the RTC, however the HAL_RTC_Init() function is returning an error. The clock configuration is this -void SystemClock_Config(void){  RCC_OscInitTypeDef RCC_OscInitStruct = {0};  RCC_ClkInitTypeDef R...

PMacp.1 by Associate
  • 1206 Views
  • 2 replies
  • 0 kudos

Atomic SPI?

I am getting two bytes making 15 bit adc result via SPI bus. Is there a way to make SPI operation atomic, what aboiut DMA. And what about code in general, how does one disable interrupts or make thing atomic.Please note, there is no rush, the CPU is ...

LMI2 by Lead
  • 1526 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.