2020-07-04 9:19 AM
I am using code generated using CubeMX to configure the RTC, however the HAL_RTC_Init() function is returning an error. The clock configuration is this -
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
}
Which I believe is correct - the Nucleo board doesn't have a 32KHz crystal so the LSI RC oscillator is selected.
The code to initialise the RTC is this -
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = 127;
hrtc.Init.SynchPrediv = 249;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
HAL_RTC_Init(&hrtc);
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
Error_Handler();
}
Both these snippets are generated by CubeMX, and the same as many examples I found with a Google search, so I must be missing a step somewhere. SysTick and GPIO configuration is working without problems, and the compiler doesn't generate any errors. Is there a simple way to debug what is happening in the HAL_RTC_Init() function to find my error, or have I overlooked a configuration step? All suggestions gratefully received.
2020-07-04 9:54 AM
You/CubeMX shouldn't be calling HAL_RTC_Init twice. Might be the source of the error.
> Is there a simple way to debug what is happening in the HAL_RTC_Init() function to find my error...
Set a breakpoint and step through the code to see where and why it returns the error and go from there. The HAL source code is part of your project.
2020-07-04 10:03 AM
Thanks for spotting the duplication, that was legacy from some earlier experimentation, but unfortunately not the source of my problem. I was rather hoping that I have missed a step in the configuration process that I simply can't see from being too close, but I think it is time to configure the debugger.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.