STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Linux driver for TPM ST33TPHF2ESPI

HelloI'm following the instruction of https://www.st.com/resource/en/data_brief/stpm4raspi.pdf to setup the tpm driver on my embedded linux using ST33TPHF2ESPI tpm module. But unable get /dev/tpm0 and /dev/tpmrm0 present due to driver read spi failed...

0693W000001rsgzQAA.png 0693W000001rsh4QAA.png
GChen.3 by Associate
  • 2048 Views
  • 1 replies
  • 1 kudos

Implement PWM dithering 1 bit

Hi I am working on stm32f070. The STM32F0 system clock = 48MHz,I need to set the PWM frequency on 23437Hz.Therefore, PWM resolution = 48MHz / 23437Hz = 2048 (11bit)​How to use PWM dithering technique to reach 12-bit resolution on PWM frequency 23.4KH...

sam_cheng by Associate III
  • 3177 Views
  • 5 replies
  • 0 kudos

STM32F7 FMC Nor Flash Problem

Hello everyone,I have designed a board with STM32F750N8, 22 Bit Parallel Nor Flash, 13 Bit SDRAM, QSPI Nor Flash.Now i am trying to read, write data, read device id from fmc nor flash (other memories not enabled). But when i try to read device id, ge...

want to zip and unzip assets in stm32f4 MCU

Hi All,I am using STM32F429ZIT6 MCU. And we were planning to zip the assets and unzip them inside MCU. Please can anyone suggest the best starting point for good libraries which can do this.Thanks,krishna

Kpodu.1 by Associate II
  • 5521 Views
  • 4 replies
  • 0 kudos

ADC Error to HIGH.

Hey Everyone;I`m working with the STM32L031K6T6 in a project that I require 2 ADC channels. The ADC look to be working with a huge measurement error:Project description:Signal Type: Sinusoidal ( 1Vpp) with offset of 1.492 ( Offset provide by independ...

0693W000001t4AZQAY.png 0693W000001t4BvQAI.png 0693W000001t4CAQAY.png 0693W000001t4D3QAI.jpg
CMart.3 by Associate II
  • 2182 Views
  • 3 replies
  • 0 kudos

STM32L496VGT6 - Does anyone know for a fact that receive works on USART3? Please no "assumptions" -- I already did that.

Transmit works to PC via FTDI cable.Receive works from PC to PC (TXRX looped) So FTDI transmit working.Receive generates no interrupt.Receive sets no status.Receive data register remains zero.As GPIO, receive pin sees signal.It is as if the alternat...

How to "printf" on STM32F746-DISCO ?

I followed the step on the following video without the configuration of SD card. (I don't need it)https://www.youtube.com/watch?v=4f-leBIJkRY​Whenever transmitting 10 characters, the program broke bown on 11-th character as below: printf("12345678901...

Ellaine by Associate II
  • 2874 Views
  • 5 replies
  • 0 kudos
Axcvn.1 by Associate II
  • 4876 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.