STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Debug

Hello STM community, I'm using a STM32 L476RGB NUCLEO with a XNucleo 53l0a1 I want to make the process of calibration but I have a problem when I compile my main program i get this error showing anyone know what i should do? you can see the screenTha...

MSAMB.1 by Associate III
  • 1407 Views
  • 1 replies
  • 0 kudos

Resolved! Probleme on getting clock signal on SPI slave device,

Hi ,i have a problem with SPI slave device, it doesn't receive the clock signal from stm32f103 (Master), i have configured the baud rate correctly : 72Mhz/32 (SPI1), which is inside the range clock freq of slave device, CS pin is active low so when i...

0693W000003BDzzQAG.png 0693W000003BDzpQAG.png 0693W000003BDzfQAG.png
SIDRI.1 by Associate III
  • 1068 Views
  • 1 replies
  • 0 kudos

Communication with interrupt between 2 cores

Hello,I am trying to communicate with interrupt between the Cortex M4 and M7. I tested the HSEM but, maybe I'm wrong, the semaphore locks a process when it waits for it.Thanks for you help

OADDI.1 by Associate II
  • 2001 Views
  • 3 replies
  • 0 kudos

Timer for generating 1us tick

I'm using STM32F108RG on 48MHz clock configuration.I need to generate a 1 micrososeconds timer tick on it, for driving an output pin interfaced with a 3rd party device. Using PWM is not an option available.I tried configuring TIM3 with following para...

SShid by Associate III
  • 8532 Views
  • 10 replies
  • 0 kudos

stm32 IAP Binary problem

I am getting this error while debugging "Break at address "0x20004000" with no debug information available, or outside of program code". I am attaching main and linker file. How to solve this? Thanks in advance..

STM32L0 ADC voltage calculations

I have been trying to calculate voltage of the battery connected to ADC_IN7 of STM32L010K8. I have connected a battery to it via voltage divider. When I read the ADC I get raw values of 1948 for applied voltage of 3.7V. After going through the datash...

ARai by Associate II
  • 3985 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.