STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L475VG DAC configuration issue: no signal observable on GPIO?

I'm trying to get a very simple example working with the DAC on the STM32L475VG in the B-L475E-IOT01A development board. I've generated the code below with STM32CubeMX for use in STM32CubeIDE. I can see the DAC register values changing, and LD1 blink...

BHM by Associate II
  • 3053 Views
  • 5 replies
  • 0 kudos

SPI DMA Stream Seems to Eventually Freeze

Hi,I'm using CubeMX generated HAL drivers to use SPI in DMA mode. In my particular situation, we are sending a small amount of data (3 bytes) very often over the SPI interface. The data transmission works fine most of the time, but sometimes (as litt...

Drew M by Associate II
  • 2346 Views
  • 4 replies
  • 0 kudos

Hello everyone, I am using stm32f207zg with usb ttl converter with ftdi chip. I want use the usart1 for communication with PA9 e PA10 pins as TX and RX of usart1. I use as virtual terminal, termite, and when i play the program, appear weird characters.

#define RCC_CFGR *((long*)0x40023808)#define RCC_CR *((long*)0x40023800)#define RCC_AHB1ENR *((long*)0x40023830)#define GPIOC_ODR *((long*)0x40020814)#define GPIOA_MODER *((long*)0x40020000)#define GPIOA_OTYPER *((long*)0x40020004)#define GPIOA_AFRL ...

FCa.1 by Associate II
  • 4183 Views
  • 11 replies
  • 0 kudos

Why can not change DBGMCU->CR in STM32F103

I'm use STM32F103C8T6. I use DBGMCU->CR = DBGMCU_CR_TRACE_IOEN to change the value of DBGMCU->CR, but the operation is failed after POR, the register is alway read 0.I suspect that the cause of this problem is the the debug component is not be powere...

Bpan.1 by Associate
  • 2089 Views
  • 3 replies
  • 0 kudos

Resolved! Slow ADC with DMA

Hi guys,I'm using STM32F767 nucleo with STM32Cubeide. I've configured an ADC to operate with DMA at a sample rate of 1.8Msps. I've calculated this sample speed by:HCLK = 216MHzPCLK2 = 108MHzPrescaler of 4 : ADCCLK = 27MHzResolution (12bits + 3)Theref...

CDyer.1 by Senior
  • 2429 Views
  • 7 replies
  • 0 kudos

obtain the data from camera for cmsis-nn

Hi, I want to do a computer vision application on stm32f407VG discovery board. I have an CNN code with cmsis-nn library. My challange is that Using the camera datas as an input. But i need rgb data as 1 dimentional array. How can save the image in a...

FÇeli.1 by Associate
  • 711 Views
  • 0 replies
  • 0 kudos

Resolved! PD0 internal pull-up working weird with PD1 internal pull-up. in stm32g071cbu MCU. Can it be an MCU internal problem?

We developed a new board with STM32G071cbu MCU which we already successfully used in our previous project.In this project we desided to use buttons with internal MCU pull up. Buttons connection is actually very simple:So in this configuration with pu...

ADovn.1 by Associate II
  • 3335 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.