STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART RX ambiguities

Hello,i'm trying to use UART with STM32F767ZI Nucleo board. I'm using the following simple code (the essential parts):/* USER CODE BEGIN PV */ uint8_t a[] = {0x81, 0x00, 0x00, 0x00, 0x00}; uint8_t b[] = {0x00, 0x00, 0x00, 0x00, 0x00}; uint8_t error[]...

0693W000003PrD0QAK.png
AMerc.4 by Senior
  • 1508 Views
  • 1 replies
  • 0 kudos

Hello Guys, I have got problem with debugging. While running debugging the error comes up: 120/5000 120/5000 Error message from debugger back end: localhost: 61234: The system tried to join a drive to a directory on a joined drive

I am using nucleo f401-re and I am a beginner. I have run couple of simple programs, and till today it works fine. Does anyone had similiar problem?Thanks in advance

MOrsz.1 by Associate
  • 1055 Views
  • 1 replies
  • 0 kudos

Nucleo-F767 + Adafruit uSD example doesn't work

I'm going back to basics with the uSD so I bought the Adafruit shield required for the example that comes with the CubeF7. Well it runs a few lines of code and then locks up and STLink wont connect! Any clues as to what to look at or what's going wro...

Vbat current consumption issue in run mode

Hi,we are using STM32f373, with VBAT powering by Li 3V battery, when we disconnect VDD (3.3V), the current consumption from the battery is 1uA, when we supply VDD, the current consumption jump to 29uA. in "run mode" (VDD supplied) If we disconnect ...

ABinu.1 by Associate
  • 800 Views
  • 0 replies
  • 0 kudos

Use of LSE for TIMxx on STM32L4

Hello,Is it possible to use the LSE clock 32.768 KHz as external clock source for TIMxx on the STM32L4 series ?I have an application running on STM32L1 and using external ****-source mode 2 for TIM10 as described in Figure 131 of the Reference Manual...

Zafi by Associate II
  • 1330 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.