STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! what is the crystal oscillator frequency of UART of STM32f103CB

Hi,​I just read an article mentioned that micro controller will limit (or do smthing) to lower down the frequency of crystal oscillator to match the multiply number of 9600 for UART, is that right?​So if I'm using PLL to boost CPU frequency from 8M t...

Olly Kao by Associate III
  • 4559 Views
  • 3 replies
  • 0 kudos

STM32H7 DMA memory to GPIO port

Has anyone got working example code they could share of setting up DMA to transfer from memory to a GPIO port on an H7 (Nucleo-H743). I've read AN4666 and can get the example working on a L476 but none of the many variants I try on the H7 work. The...

RCC HSE (8.000 Mhz Crystal) STM32F411E-DISCO, Running Slower

Hello I am using the STM32F411E-Discovery board, selecting the HSE ceramic resonator, which is installed on the board as 8.000 Mhz Crystal, as clock source for a 1 sec interrupt with TIM2. I am using STM32CubeMx BUT INSTEAD OF HAVING 1 SECOND INTERRU...

JVela.1 by Associate
  • 1407 Views
  • 3 replies
  • 0 kudos

Uart DMA RX problem

Hi there !I use uart with DMA for receive data from (right now) pc and STM32F051 discovery board, everythingh work bettere if i send all data, but if i send less data stop the work . Let me explain i need the send 180 bytes from pc to discovery boa...

SGian.1 by Senior
  • 1188 Views
  • 2 replies
  • 0 kudos

We are using this ic STM32F103VET6 and Oscillation of 8 MHz Crystal with through capacitor of 22pf i am not getting the Oscillation from the microcontroller ?

We have two same design Board, one is fabricated in last year, another one is this year fabricated boards and i loaded same code for both boards.Achivally this year what i fabricated with little changes on the Connector side and we are used buffer ic...

SMudi.1 by Associate
  • 1459 Views
  • 2 replies
  • 0 kudos

Changing data advertisement frequency on BlueNRG DK example

Hello, I am using the example code BLE_Throughput from the BlueNRG-2 DK to program a PCB. The example is working fine but the frequency of advertisements is too high for what I need and I could not find in the code where can I change it. Could someon...

CFred.1 by Associate
  • 896 Views
  • 0 replies
  • 0 kudos

CAN mystery. Receiving messages but not able to send

Hi.I have a program that sometimes fails to send data on CAN but still receives them correctly.This is on an STM32L462 using 1.4.2 IDE and latest API.For some unknown reasons, at one moment, out mailboxes never empty. It can be anytime from right upo...

STM32H745 Maximal performance configuration

I'm working in a project that involve a thermal camera image processing.I need to process a buffer of 384*288 (16bits) in fastest way possible.I'm using the 480Mhz VCO template to set the procesor in 400Mhz (Cache enabled).I already did some code op...

Jvela.11 by Associate II
  • 1997 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.