STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Which JSON library is preferable for STM32F769 DISCO board?

Hello,I'm working on a project on STM32F769 DISCO Board in which I need to read and parse data from a .json file (3kb). I tried using Nlohmann JSON.hpp library for data reading and parsing and, even if I do not have compilation problems (except for a...

PDe N.1 by Associate
  • 1024 Views
  • 0 replies
  • 0 kudos

STM32L072 not receiving UART1 interrupt in Stop Mode

Hello all,I want to use STM32L072 in Stop mode. But, it should receive interrupt UART interrupt while being in the stop mode. It is not receiving UART interrupt while being in the stop mode. Can anyone please explain the reason and the ways to solve ...

Resolved! [Solved]Problem with Usart Irq

Hi at all,Sometime happens that usart2 irq freeze and HAL_UART_RxCpltCallback isn't called.From this moment I can send data (I use blocking instruction HAL_UART_Transmit), but don't receive any.When this happens, HAL_UART_ErrorCallback don't called t...

SDall.11 by Associate III
  • 2374 Views
  • 4 replies
  • 0 kudos

I2C CLOCK CHOOSE SYSCLK AND PCLK1

HEY I am having stm32f767zi. As datasheet has mentioned it has 216MHZ CLOCK. NOW PCLK1 is 54Mhz max. So stm32cubemx has 3 option for i2c. SYSCLK , HCLK AND PCLK1. By default stm32cubemx selected pclk1 for i2c which is 54mhz. so can i use sysclk for i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.